5 Reasons to Use AC Drives with Safety

5 Reasons to Use AC Drives with Safety

Boost productivity, simplify systems and optimize performance by using AC drives that provide advanced safety over Ethernet.

By Andy Gagnon, Product Manager and Ryan Miller, Product Management Specialist, Rockwell Automation

If you still only view safety simply as a matter of compliance, you’re missing the bigger picture in these times of smart manufacturing.

Smart, networked safety can give you measurable business benefits. And it can push the boundaries of what’s possible in your operations.

Low-voltage AC drives with integrated safety are a perfect example of what networked safety can do. When connected to a safety programmable automation controller (PLC) over Ethernet®, they can give you more insights into your operations, reduce system wiring and components, and add precious minutes back to production. And yes, they can also help you be compliant — and maybe even reduce safety risks.

To put this in context of the bottom line, here are five business cases for using AC drives with integrated safety.

1. Increased Productivity

Lockout/tagout (LOTO) has been a core element of industrial safety. But it also can constrain productivity.

AC drives with integrated safety let you to use safety functions in place of LOTO procedures in certain instances. Safety functions — such as safe limited speed, safe torque off and safe brake control — can help your workers service equipment in a fraction of the time and still be compliant.

Consider a task such as cleaning augers and rotating drums. Using LOTO procedures, workers must continually start and stop the assets to clean them. Safety functions such as safe limited speed and safe direction lets worker clean the equipment while it rotates at a slow speed.

2. Enhanced Safety

Workers sometimes bypass LOTO procedures to stay productive. That creates serious safety risks. AC drives with safety functions that help workers to more quickly service machines can reduce incentives for bypassing safety procedures.

Also, safety functions can support passive safety systems to reduce risks for new workers. Passive safety systems perform functions with little or no worker effort required. This can help mitigate the risks of inexperience, such as workers placing their hands in hazardous areas.

3. Reduced Complexity

Traditional safety products are hardwired separately from a standard controller and can require extra hardware like safety relays. A networked safety product such as an AC drive with integrated safety can share the same Ethernet network as a standard controller and reduce the need for added hardware. This can simplify your system and reduce its costs.

Networked safety and control products also can be programmed, configured and maintained in one software environment, further reducing complexity.

4. Better Insights

An AC drive with integrated safety can give you access to rich analytics to help improve your performance.

For example, you can track the time, location, frequency and duration of when the drive’s safety functions are being used. This can help you better track safety-related downtime and identify changes to improve uptime. Drive diagnostics can also help you see where safety-related failures occur to speed up troubleshooting and recovery.

5. Greater Flexibility

An AC drive with integrated safety can grow and change with your business. For example, you can use the advanced safety functions later if they’re not needed today. The drive delivers integrated safety through a card that you can add at any time.

You can also easily change the drive’s safety applications as your requirements evolve over time. A hardwired safety solution can require complex planning and rewiring to meet new safety requirements. However, a networked solution only requires updating code in your safety PLC.

Safety as a Business Enabler

Networked safety products can do more than compliance. They can help you maximize the performance of your business. If you want to digitize your operations, networked safety products can be part of that.

Learn about low-voltage AC drives with integrated safety. 

 

 

 

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.

Contact

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Latest News

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.