Process System Cuts Hardware Cost by 25%

Process System Cuts Hardware Cost by 25%

Challenge

  • Deploy a controls system with significant cost savings

Solutions

  • EtherNet System with Allen-Bradley® Flex™ IO – The new process system included roughly 6,000 I/O points comprised of digital, analog and DeviceNet I/O
  • The project team changed the design from ControlNet with rack I/O to an EtherNet system with Allen-Bradley Flex I/O
  • Solution Connects Flex/IO to Ethernet – The new design provided a 25% controls hardware cost savings compared to the old design
  • The new design reduced the network types in the plant, decreasing training requirements and spare parts needs
  • The new design allowed for additional cost savings during installation due to lower-cost Ethernet media run

Results

  • Significant contribution – The collaboration between Rockwell Automation and Polytron, Inc., helped deliver significant cost savings
  • Results as anticipated – Able to save money while improving control system performance
  • Successful collaboration between Polytron and the food manufacturer identified the pros and cons of all options and helped ensure that the project’s requirements were met

A food manufacturer discovers that the right I/O hardware solution for its controls system can create significant cost savings

Reducing cost is always one of the top priorities for every automation integration project. Combine this with the economic downturn limiting capital investments, and it becomes even more crucial for system integrators to deliver the promised project results at the lowest possible cost.

However, how can you achieve cost reduction without sacrificing the project’s requirements? Let’s examine one project and learn how a food manufacturer teamed with Polytron, Inc., a Rockwell Automation qualified Process Solution Provider, to save money while improving control system performance.

The new process system for the manufacturer’s state-of-the-art greenfield facility included roughly 6,000 I/O points comprised of digital, analog and DeviceNet I/O. Polytron provided controls automation and manufacturing execution system (MES) design services for multiple process and packaging lines.

Polytron analyzed the manufacturer’s planned I/O hardware design to ensure it provided the best value for the project. This analysis of the new design, resulted in an approximate 25% cost savings for the controls hardware.

As the system’s mechanical design evolved, additional I/O had to be added to support the increased processing capabilities requested by the manufacturer. This increased the I/O by more than 20%, from 6,000 I/O points to more than 7,000. This increase of scope typically creates budget issues for a project.

However, the new design allowed the additional scope to be delivered at a 10% cost savings of the original controls hardware budget.

The Technical Approach

The originally planned control system consisted of connecting eight Allen-Bradley® ControlLogix® programmable automation controllers (PAC) from Rockwell Automation to Remote I/O racks via ControlNet.

At the start of the detailed design phase, the planned design and customer requirements were analyzed. This analysis included use of the Rockwell Automation Integrated Architecture Builder (IAB) software and EtherNet/IP Capacity Tool.

The IAB provided a Bill of Material based on design information entered into the IAB software, such as I/O type, number of nodes, I/O points connected to each node and network type. This, in turn, allowed pricing to be obtained for each design option. “What if” scenarios were then developed to determine the cost for each configuration option.

The EtherNet/IP Capacity Tool was used to determine the predicted performance for each EtherNet/IP network option. The tool calculated the predicted network bandwidth, number of connections used and remaining connections available, based on the type and number of nodes on the network.

This information allowed Polytron to determine the network layout and connection media (fiber, copper) most suitable for the project. In addition, it confirmed that the EtherNet/IP network ring had enough bandwidth available to provide the required communications if one of the paths became accidentally disconnected.

The IAB and EtherNet/IP Capacity Tool software tools helped optimize the I/O and network design. However, these tools alone can’t determine which design provides the best overall value while still meeting the project’s requirements. To do this, Polytron worked with the food manufacturer to evaluate each option’s benefits and limitations.

The Solution Connects Flex/IO to Ethernet

The project team decided to change the design from ControlNet with rack I/O to an Ethernet system with Allen-Bradley FlexTM I/O from Rockwell Automation. The deciding factors for the new design were as follows:

  • The new design provided a 25% controls hardware cost savings compared to the old design
  • The new design reduced the network types in the plant, thus decreasing training requirements and spare parts needs
  • The new design allowed for additional cost savings during installation because of less expensive Ethernet media run compared to ControlNet

Every design option typically has drawbacks that the project team needs to accept or find an alternate solution. In this project, the system included safety and other nonsafety I/O connected via DeviceNet.

The new design required that the rack-mounted Allen-Bradley 1756-DNB cards, used for connecting to the safety I/O, be replaced with stand-alone Allen-Bradley 1788-EN2DN modules because the field racks were to be eliminated.

This was a good solution for the nonsafety I/O. However, the 1788-EN2DN modules aren’t rated to connect to safety I/O. To solve this problem, a CLX rack with a 1756-DNB card was added in each Allen-Bradley CENTERLINE® Motor Control Center (MCC) with IntelliCENTER® for connecting the MCC’s drives and starters back to the Allen-Bradley GuardLogix® safety controller.

Make the Most of a Project

For any automation integration project, initial design assumptions made during the early phases should be revisited during start of detailed design to ensure that the highest-value solution is implemented.

Successful collaboration between Polytron and the customer to identify the pros and cons of all options helped ensure that the project’s requirements were met.

Solution Providers

A select group of Rockwell Automation system integrators has achieved Solution Provider partnership status. This is a heightened and exclusive business relationship with Rockwell Automation. Solution Provider partners are proven, trusted and established organizations that offer extensive experience in the design, implementation, project management and maintenance of customers’ industrial control systems.

Discipline: To earn Solution Provider (SP) partner status, integrators must possess high corporate standards, financial stability, proven methodologies and competency using Rockwell Automation technologies.

Credibility: SPs are well-established organizations that offer extensive experience in advanced automation solutions. They have been trusted advisers for their customers from initial design and consultation, system development, through the commissioning of comprehensive Rockwell Automation solutions.

Expertise: Whether your need is in design, project management, implementation or manufacturing systems maintenance, SPs possess the industry knowledge, domain expertise, resources and skills to deliver world-class solutions.

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.