PowerFlex 750-Series Configuration and Startup

Description

This course (CCA182-EL) provides you the ability to properly install a PowerFlex® 750-Series drive, start up the drive, and configure drive parameters to meet application-specific needs. Throughout the course, you will have the chance to use a variety of software tools, including:

  • The A6 LCD HIM
  • Connected Components Workbench™ software
  • DriveExecutive™ software

Objectives

  • Verifying the PowerFlex 750-Series Drive Installation Environment
  • Verifying PowerFlex 750-Series Drive Wiring and Grounding
  • Locating and Modifying PowerFlex 750-Series Drive Data Using the A6 HIM
  • Configuring EtherNet/IP Communications for a PowerFlex 750-Series Drive
  • Locating and Modifying PowerFlex 750-Series Drive Data Using Drive Software
  • Starting Up a PowerFlex 750-Series Drive
  • Interpreting PowerFlex 750-Series Control Block Diagrams
  • Controlling PowerFlex 750-Series Drive Operation

Prerequisites

To successfully complete this course, the following prerequisites are required:

  • Working knowledge of electricity, and knowledge of electrical and industrial safety (including PPE requirements and safe practices)
  • Completion of the AC/DC Motors and Drives Fundamentals course (Course No. CCA101) or equivalent experience

Who Should Attend

This course is for individuals who need to configure and start up PowerFlex 750-Series drives.

Register

Register for one free e-learning course through June 30, 2020 and start learning today.

Start Learning Today!