Studio 5000 Logix Designer Level 3: Basic Ladder Logic Interpretation

Description

This course (CCCL21-EL) is a skill-building course that provides you with a more detailed understanding of Studio 5000 Logix Designer® ladder logic instructions and terminology. This course also provides you with the resources required to interpret ladder logic instructions for any Logix5000™ controller. You will have an opportunity to use the Logix Designer application
to perform basic software tasks to meet the requirements of a given functional specification. In addition to using ladder logic, you will be introduced to ladder logic techniques, established standards, and common rules for interpreting ladder logic.

Objectives

  • Interpreting Program Control Instructions in a Studio 5000 Logix Designer Project
  • Interpreting Timer and Counter Instructions in a Studio 5000 Logix Designer Project
  • Interpreting Math Instructions in a Studio 5000 Logix Designer Project
  • Interpreting Comparison Instructions in a Studio 5000 Logix Designer Project
  • Interpreting Move Instructions in a Studio 5000 Logix Designer Project
  • Interpreting Copy and File Fill Instructions in a Studio 5000 Logix Designer Project

Prerequisites

To successfully complete this course, the following prerequisites are required:

  • Completion of Studio 5000 Logix Designer Level 1: ControlLogix System Fundamentals (Course No. CCP146) or equivalent experience
  • Completion of Studio 5000 Logix Designer Level 2: ControlLogix Maintenance and Troubleshooting (Course No. CCP153)

Who Should Attend

Maintainers who need to interpret ladder logic using the Logix Designer application should attend this course.

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.