Device Configuration
How do I open the Device Configuration dialog box?
Right-click a device in and select
FactoryTalk Linx
BrowserDevice Configuration
.The
Device Configuration
dialog box includes tabs that contains the port and network configuration of a device. They are Internet Protocol, Port Configuration, Network Configuration, and IP Mode.
CONSEIL:
- This option is grayed out if the user has no permission inFactoryTalk Securityto access the device configuration or if the advanced option has disabled it, or the device is in Explicit Protected Mode.
- Users need to set permission inFeature Security Properties>Policy Settings>Open Device Configuration.
The button/option is only available when:
- The device supports this function
- Advanced Settings>Enable Device Configurationis selected.CONSEIL:Users need to set permission inFeature Security Properties>Policy Settings>Modify Browser Settingsto access toAdvanced Settings.
- The user is permitted access throughFactoryTalk Security.
- The device is in unprotected mode.
These tabs are not available in
FactoryTalk Linx
Network Browser for all devices.
CONSEIL:
To display the device icon correctly, please make sure the corresponding device description file is installed.
Fournir une réponse