Achema

Frankfurt, Germany • 11 – 15 June 2018

Hall 11.1 | Stand E27


World Forum and Exhibition for the Process Industry


Join us at Achema to see how you can address the challenges of establishing, running, maintaining and securing your digital factory.

Our modern PlantPAx Distributed Control System (DCS) reduces implementation time and helps you make better, faster decisions to respond more quickly to the demands of customers and fast-changing specifications.

Let us show you what a modern, integrated DCS can do for you and your Connected Enterprise.

ACHEMA 2018 will bring together more than 166,000 participants from 100 different countries, with 30,000 top and middle management executives. Join us as we help define the future of industry.

Local Events

Dates

11 – 15 June 2018

Location

Frankfurt, Germany

Bio Tech Demo Session

At our booth we will be showcasing an innovative, single-use bio reactor. Integrated into our digital DCS and using an S88-compliant batch solution, it can be driven by a plant-level batch system and links seamlessly in to ERP suites.

The quick connect/disconnect features of the single-use bio reactor are also integrated into our digital DCS, which delivers higher operability combined with increased visibility. Another major step towards the digital plant of the future.

Book your bio reactor demonstrations slot now to get a personalized, one-to-one demo and see how our solutions can help define your next innovation

Rockwell Automation Single Use Biotech demo – Hall 11.1 | Stand E27.

Key topics

This year's event includes

Process Automation: Instrumentation, control and automation technology

Safety Technology: Industrial and labour safety issues

Environmental ProtectionIndustrial water management

Flexible ProductionPharmaceutical manufacturing

MACHINE PROFILES

See our solution in action around the event. Read the machine profiles and then visit these stands to see the machines in action.

ASOS — Hall 6.1 | D41

BAUSCH & STRÖBEL MASCHINENFABRIK — Hall 3.0 | D3 — DDM9105

DINNISSEN — Hall 5.0 | D17 —  All-in-One Mixing concept

FELUWA — Hall 8.0 | H93 — EcoTrans MULTISAFE

FRYMAKORUMA — Hall 5.1 | D33 — Dinex

GABLER — Hall 3.0 | F99

IMA/GIMA — Hall 3.0 | F49 — EVO FLEX ROTARY

IMA/GIMA — Hall 3.0 | F49 — iQ FLEX

ZELLWAG PHARMTECH AG — Hall 3.0 | B25 — Z-810 Rx six-axis filling and closing system

ZETON — Hall 9.1 | F30 — High-Throughput Catalyst Testing System

Conference

Panel Presentation: ‘Cyber security - why and how?’

Industry 4.0 with the IoT have been pushed very hard by governments and manufacturers, who are highlighting the benefits and advantages of an even more digitalised world. But what are the pros and cons?

From a security perspective it is clear we need to increase the level of protection.

How? It has to be a systemic approach, which includes ALL the components and ALL the people involved.


Join us at the Achema conference!

Where: CongressCenter Messe Frankfurt | Room CMF - Illusion 1
When: Thursday 14th June 2018 | 10:30-12:30 h and 15:00-16:00 h
Who: ISA & Rockwell Automation
Speaker guests: Rockwell Automation, Microsoft, Cisco, Panduit & Claroty

Maximise Productivity And Help Minimise Risk

Rethink what to expect from your DCS

A modern distributed control system (DCS) is built using plant-wide control technologies. Today, process control, discrete control, power control and safety control no longer have to be tied to separate technologies and networks. Producers can now choose to implement an integrated plant-wide control system.

Download Brochure

PlantPAx: Simplify and Leverage Virtualization

PlantPAx Virtual Image Templates from Rockwell Automation deliver the core system elements as pre-configured, drop-in templates on a USB hard drive.

Download Brochure

Visit our Process Solutions page for information on how to achieve your production goals, meet customer demands, and stay ahead of the competition.

Event Location

Exhibition Grounds of Messe Frankfurt GmbH

Ludwig-Erhard-Anlage 1
60327 Frankfurt am Main
Germany

View location on Google Maps.

Visit the venue's website.


To find out more about the event, please visit the ACHEMA 2018 website.