Increase the Up-Time of

Important Plant Assets

How to Reduce Unexpected Downtime with Low Harmonic Drives

Low harmonic drives using active front-ends are an excellent way to meet the requirements of IEEE-519 and are becoming widely accepted, but some manufacturers see them as complex and question whether they will lead to more unplanned down time. Advances in the predictive maintenance algorithms and adaptive control on some drives provide a significant improvement in the up time of a system.

Join us to learn about:

  • Benefits to using drives with built-in harmonic mitigation
  • How predictive maintenance features embedded in drives can reduce unexpected downtime
  • How to comply with the requirements of IEEE-519