How The Danish Navy Put New Wind In Their Sails

How The Danish Navy Put New Wind In Their Sails

Challenge

  • After 15 years of active service, the Danish Navy needed to re-fit and modernise technology aboard the Absalon-class support ship

Solutions

  • ThinManager – Delivers improved performance by adding an additional layer of supervisory functionality. Provides control and security that is scalable for the vessel’s needs.
  • FactoryTalk View SE (HMI software) – Delivers crew a more concise and clearer content system (specific to vessel’s situation and / or rank)
  • IPMS (Integrated Platform Management System) – The FactoryTalk application that compiles more then 8000 signals into comprehensive mimic displays for overview and control
  • Rockwell Automation PartnerNetwork – LOGIMATIC, a Rockwell Automation Systems Integrator, providing design, services and support

Results

  • Reduced Downtime – Upgraded systems and simplified terminals are a ‘plug-in’ solution resulting in minimal downtime at sea
  • Improved Efficiencies – HMI software helps crew quickly shift between tasks and monitoring systems. A ‘connected’ vessel that provides crew with graphical user terminals to quickly address issues / tasks from anywhere
  • Enhanced Security – The most robust security protocols to both control the flow of information and fend off any cyber-attacks

LOGIMATIC designs new marine tech solutions, giving sailors faster reacting terminals and tools

Not many of today’s best practice technology stories start with naval ships, life-threatening situations and the potential of war. But in the case of the Danish Navy and its need to upgrade vessels in their elite Absalon-class support fleet, this is exactly the case.

Understanding the specific needs of the armed forces can be difficult for even the best ‘civilian’ technology architect to tackle, however LOGIMATIC, a leading system integrator had extensive experience working with the Navy. Together with long-time ally Rockwell Automation, they faced the first of the Danish Naval flexible support vessels when it arrived into dry dock for a complete technical overhaul.

They knew they would have to not only think and act like they were sailing the high seas themselves, but to push the boundaries of marine technology.

Fifteen years at sea

Built in 2003, the Danish Navy ship HDMS ABSALON (L16) was scheduled to have its automation and remote control system completely replaced after a 15-year lifespan. The situation called for nothing less than a complete modernization of the ship’s entire technical infrastructure.

Running the ship’s outdated ‘thick’ system was not only excessively expensive to maintain, but in many cases had become so obsolete that it was no longer updatable. User terminals around the vessel with banks of screens controlling different functions such as fire management, warning systems, camera monitoring and alarms had become a labour intensive task to maintain.

It had become critical to overhaul this aging infrastructure to confirm that serving naval personnel could access the right application from the right location at the right time, with a modern visualisation system which would not only improve the user experience, but also to save time and potentially save human lives.

"Clearly the ship’s technical abilities were antiquated and needed to come into line with more modern capabilities,” explains Mathias Jensen, Project Engineer, LOGIMATIC. “The Danish Navy was keen to find new flexible, yet resilient, solutions for their personnel which could be easily implemented and activated.”

Course set for updates

LOGIMATIC, knew the situation required a “leaner” system which would connect the entire vessel in a way where content could be managed, delivered and shared with terminals anywhere across the ship via any crew member.

However demonstrating to the Danish Navy that this system was the best plan of attack was not as easy as a standard pitch. So LOGIMATIC decided to go the extra mile – they custom built a dedicated, fully operational proof of concept lab where their proposed systems could be tried and tested first-hand.

After in-depth consultations with the navy, including time spent inside the lab, LOGIMATIC’s recommendation was to design and implement ThinManager, the simplified technical architecture from Rockwell Automation which simplifies management of hardware, applications and visual sources. Having been impressed with much of the pre-work performed with ThinManager during this consultative process, navy personnel readily agreed to set sail.

“We spent a huge amount of time together with the Danish Navy inside our concept lab, constantly reviewing designs and trouble-shooting potential issues” continues Mathias Jensen. “We knew that we would have a limited amount of time on the ship itself, so it was critical that all parties felt comfortable with our plan. The concept lab was an excellent way to do so.”

Once the project was officially given the green light, it quickly became necessary for LOGIMATIC to go beyond the land locked lab and set out to sea with the ship’s crew, regardless of the 20 year history working with the Danish Navy. They needed to gain a stronger first-hand understanding of the pain points, naval requirements and best-case solutions required for ThinManager implementation.

Everything considered ‘standard practise’ with civilian clients went overboard when the LOGIMATIC team began working directly with the crew of the naval support ship. Seemingly simple issues such as switching between screens, pressing a button or even the size of a standard mouse needed to be considered as a potential matter of life or death.

By gaining a deeper level of understanding and appreciation of the conditions that the IT infrastructure would need to perform under, the LOGIMATIC team developed a specifically tailored ThinManager solution. Purpose designed software was programmed into carefully considered hardware, with multiple sources integrated into single display terminals instantly capable of reading and reacting to constantly incoming data from all over the ship’s IP cameras, FactoryTalk View SE SCADA system and other third-party software packages.

Built in 2003, the Danish Navy ship HDMS ABSALON (L16) was scheduled to have its automation and remote control system completely replaced after a 15-year lifespan.

Sailing on a technology wave

Once the initial system was installed, the LOGIMATIC team continued to sail with the Danish Navy onboard the newly refitted HDMS ABSALON (L16). Testing and refining the infrastructure in real life scenarios throughout Norway and Scotland allowed for a collaborative effort to hone systems, hardware and protocols.

What was a heavy system of aged hardware and countless sub-systems had been upgraded with customised server based software and virtual machines at each user terminal. Easily accessed by assigned personnel and seamlessly delivering the content that is most relevant to each situation, the HDMS ABSALON (L16) had taken a giant leap forward from its fifteen year old self that had been hoisted into dry dock only months earlier. So-much-so that sister ship HDMS ESBERN SNARE (L17) was quickly approved for a complete technological overhaul.

“Any unforeseen downtime at sea can be dangerous, especially in potential combat situations,” shares Søren Præsius, Project Manager, Electrical Power and Automation, Danish Ministry of Defence Acquisition and Logistics Organisation.

“Having the ability to work on terminals with a consistent, lightning-quick speed can literally be a life or death situation. Our crew members are now empowered to quickly act, under any level of stress, with a system that is consistent and intuitive to use.”

Lowered cost of operation is also one of key benefits the Danish Navy has experienced as a result of the ThinManager implementation. Excessive and expensive-to-maintain hardware has been removed in place of more modern, efficient controls together with HMI software. ThinManager is also scalable to allow for any number of adaptations and necessary changes over the coming years, which translates to a reduction in costs especially when compared to the legacy system.

Security in any armed forces is paramount and nothing more so than a naval vessel at sea or dockside where all precautions need to be taken against malfunctions and the threat of outsiders bringing computers or USB’s onboard for example.  LOGIMATIC implemented the ThinManager system to employ the highest of security measures. While the new system is still an ‘open system,’ the architecture makes executing protective means far more efficient and effective.

“We’ve seen a very positive impact on the entire Danish Navy via of this project,” says Søren Præsius.

“The new technology provides a blueprint for improvements to be made throughout the rest of our fleet. The successful upgrades to both HDMS ABSALON and ESBERN SNARE has paved the way for enhancements to three of our Naval frigates. We’re looking forward to seeing what else we can accomplish together.”

Logimatic, Sofiendalsvej 5B, 9200 Aalborg SV, Denmark
www.logimatic.dk
lmc@logimatic.dk
+45 9634 7000

Logimatic

Partner Company Statement. Logimatic is a Danish engineering and technology company, specializing in software and automation solutions. For more than 30 years Logimatic has helped businesses advance by optimizing and streamlining internal processes. Logimatic’s in-house developed solutions are tailored for the maritime, production, utilities, logistics and energy sectors – and their consultancy services are based on profound industry expertise and tailored to meet each customer’s individual needs.

The results mentioned above are specific to the Danish Navy’s use of Rockwell Automation products and services in conjunction with other products. Specific results may vary for other customers.

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.