Bring Greater Productivity and Flexibility to a Connected Enterprise through Reliable I/O Solutions

Bring Greater Productivity and Flexibility
On-Demand

Duration

60 Minutes

Language

English

FLEX 5000™ I/O is built on a higher-speed connectivity and expanded bandwidth platform to deliver increased amounts of data back to the controller. This helps future-proof control systems for a Connected Enterprise. During production, the modules can reduce costly and unplanned downtime, especially in continuous process-control applications. Removal and insertion under power (RIUP) allows technicians to replace existing I/O, and an online change capability allows configuration of new I/O, both while the system continues to run. In addition, the flexibility to configure alarms, events and diagnostics at the channel level helps drive maintenance efficiency.

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.