The Value of Plant Safety Dashboards

The Value of Plant Safety Dashboards

We’re working on a series of blogs about the growing popularity of dashboards to help manage the massive amounts of data available to manufacturers. Last month, we covered the plant overview dashboard, and this month, I’ll explain the benefits of safety dashboards.

Downtime is a significant challenge for keeping facilities in operation, especially when it’s caused by injury. In 2017, there were around 2.8 million nonfatal workplace injuries and illnesses reported by private industry employers, according to the U.S. Department of Labor. In manufacturing, 115,550 days away from work were reported.

As we all know, downtime resulting from injuries leads to increased costs. When workers are sick or hurt, employers must pause production and spend funds to hire temporary replacements to fill in the gaps.

This is where safety dashboards come in. Safety dashboards allow plant managers to anticipate machine issues and compare the actual number of safety events against the expected number of safety events. These insights can help managers determine if they’re meeting their safety goals and inform their decisions, so they can reduce worker and machine safety events.

How Safety Data Helps Plant Managers

Overall, safety dashboards provide managers with a greater knowledge of their plant and keep them up to speed on the health of their workers. Plant managers use safety dashboards to monitor injuries daily, monthly and yearly. This data is then used when managers need to make decisions about plant safety protocols and how workers interact with operations.

Here you can see the number of injuries and days out of work for each month of the year in an easy-to-read bar graph, in addition to other relevant injury metrics (click to enlarge).

Check out the example safety dashboard to the left. Here you can see the number of injuries and days out of work for each month of the year in an easy-to-read bar graph, in addition to other relevant injury metrics.

Collecting safety data and presenting it in a convenient dashboard is helpful to managers and safety officers because it’s an easy method to organize and create meaning out of what’s happening in the facility. The data is presented in real time and can help managers set KPIs for the plant, which are then used to make a game plan for reducing lost time from safety events like injuries.

Safety information also enables managers to set goals for future years. As injury data is compiled, managers compare year-over-year injury statistics to determine if they are meeting safety goals. Proactive goal setting positions safety as a priority for the benefit of employees, productivity and overall plant operations, because it creates a benchmark to improve upon.

Safety Dashboards Help Boost Productivity

Safety analytics can be tied directly to downtime, which is why visibility into safety performance is a strong indicator of productivity. Examples of useful safety analytics include safety scores, number of days between injuries, year-to-date injuries and lost time.

If a safety score decreases because a worker pushed through a light curtain and caused a safety event, managers can drill down into the dashboard to see where the event occurred in the plant. This information opens a conversation between managers and operators to discuss compliance incidents occurring between the operator and machines. Are they being safe? Are their work methods increasing downtime?

Additionally, based on the ongoing metrics visible on the safety dashboards, plant managers can tell when machine hardware or software is going out of compliance and needs an update or modification. If a part needs to be replaced, for instance, dashboards can be set up to notify managers. These notifications help managers streamline the process to streamline how people interact with machines.

Drill Down Even Further

Beyond the initial safety dashboard, it’s possible to drill down further to reveal specifics like the causes and reasons behind safety events. Drill-down details could answer questions like:

  • Who is causing the most events? Which operator, shift or machine?
  • Which machines are out of compliance?

Answers to these questions could prompt deeper conversations that lead to greater safety and productivity optimizations like, does the operator need more training? What is causing this device to be out of compliance?

Going a step further in compliance cases, integrating machine learning could streamline machine resolutions. For example, you could set things up so work orders automatically generate and notify engineers which machines need work and when, saving further time and productivity.

Coming Up Next

Just like any of our dashboards, the safety dashboards are customizable, so plant managers and safety officers, or any plant personnel, for that matter, can design the dashboard to include exactly what they need to know.

Plant dashboards run with FactoryTalk InnovationSuite, which pulls data and presents it in mashups. In order to make data an asset, you must use tools like custom dashboards to your advantage.

If you’d like to discuss, please comment below. And to keep up the dashboard blogs throughout 2019, they’ll all be available here.

Looking ahead to next month, Jennifer Kite will explain the value of dashboards and alarm management.

Jeff Schmelebeck
Posted 24 May 2019 By Jeff Schmelebeck, Sr. Technical Consultant, Info Software, Rockwell Automation
  • Contact:

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.