New Scalable Graphic Terminals Help Increase Productivity in Smaller Applications

PanelView 5310 graphic terminals provide right-sized HMI solution for machine and equipment builders.

Machine and equipment builders are already using tight integration between the HMI and controller to help increase productivity in large applications. With the new Allen-Bradley PanelView 5310 family of graphic terminals, they can now bring these integration benefits to smaller applications.  

Click the image above to request a high resolution version.

The PanelView 5310 graphic terminals deliver the same usability benefits and enhanced integration with Logix 5000 controllers as the PanelView 5500 terminals. But the new terminals are specifically designed for applications of up to 50 HMI screens. The terminals are available in 7-inch, 9-inch and 12-inch display sizes. A 6-inch display option will be available in 2018.

“Engineers can use the PanelView 5310 family to scale a tightly integrated automation system down to smaller applications,” said Mike Moriarty, product manager, Rockwell Automation. “This can help make design, operations and maintenance tasks more efficient. For example, engineers can now reuse controller alarms without creating HMI tags, which can help them reduce configuration time.”

Companies can also use the enhanced integration to create high-speed jog buttons in place of cumbersome hardwired buttons. These auto-diagnosing buttons can interact with the controller at I/O speeds to help reduce downtime and improve productivity.

Other productivity benefits of the PanelView 5310 graphic terminals include the following:

The intuitive Rockwell Software Studio 5000 design environment allows users to create reusable faceplates, screens and custom graphics to help reduce development time. These objects seamlessly integrate with Logix add-on instructions and different user-defined data types.

Emulation capabilities allow engineers to test run projects in the development environment. This can help them make changes without using the PanelView 5000 hardware or disrupting production.

VNC connectivity allows operators to remotely monitor operations via a smartphone, tablet or personal computer. Historical-trending and data-logging features also allow operators to easily troubleshoot issues directly on the panel.

Engineers can load projects onto the PanelView 5310 graphic terminals directly from removable media to more quickly recover information and make project updates without needing to use the Studio 5000 View Designer application.

Media Contacts

Tom Spencer

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.