New PowerFlex AC Drive Option Module Provides Multiple Safety Functions on the Same EtherNet/IP Network as Standard Control

Integrated Safety Functions Option Module from Rockwell Automation helps reduce hardware and installation costs while improving productivity

AC drive applications that require safety functionality can now benefit from the integration of safety and standard control systems on a single network using one controller. The Integrated Safety Functions Option Module from Rockwell Automation offers several safety functions based on IEC 61800-5-2 standards for Allen-Bradley PowerFlex 755 and 755T AC drives. It includes the ability to monitor speed, direction and position on an EtherNet/IP network.

Click the image above to request a high resolution version.

“With integrated safety functions, manufacturers can streamline operations while creating opportunities to reduce costs and increase productivity,” said Chunbing Zhang, senior product specialist, Rockwell Automation. “The integration of the safety and standard control systems also provides operators and maintenance personnel visibility to all machine events – including safety events. This enables a quick response that allows the machine to return to full production faster.”

Networked safety solutions minimize hardware and installation costs by simplifying machine design and reducing equipment redundancies. With fewer components, manufacturers can reduce the size of panel enclosures and save valuable floor space.

Networked safety solutions also provide zone control in which one zone of the machine is brought to a safe state while other zones continue to operate. In the past, a safety event in one section of a machine could result in the entire machine shutting down, as the standard system had limited knowledge of the safety event. Integrated safety allows the control and safety systems to coexist on the same network and share data between the safety and standard applications.

As part of a comprehensive solution, a single Allen-Bradley GuardLogix controller can manage safety and standard control in one software environment, Studio 5000 Logix Designer. With no need to write and coordinate multiple programs on different controllers, manufacturers can simplify the programming process and save on training and support costs.

The integrated safety functions option module provides ratings up to and including SIL CL 3 and PLe Cat 4, when used as part of an integrated safety system that includes a GuardLogix 5580ES controller or Compact GuardLogix 5380ES controller. The option module can be added to the drive at any time.

About Rockwell Automation

Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 23,000 people serving customers in more than 80 countries.

Media Contacts

Tom Spencer
Elena Gardiner

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.