First Industrial Controller Certified to IEC 62443-4-2 Demonstrates Strengthened Security

Companies can defend their connected operations against security threats and have confidence that their control systems are designed with security in mind with the Allen-Bradley ControlLogix 5580 controller from Rockwell Automation. With new enhancements, it is now the world’s first programmable automation controller to be certified compliant with the IEC 62443-4-2 security standard.

Click the image above to request a high resolution version.

The certification by third party TÜV Rheinland confirms that the controller meets the global standard’s robust cybersecurity requirements. The controller achieved compliance with the addition of new security features to its firmware.

Security features within the ControlLogix 5580 controller include:

• User identification and authentication
• Continuous monitoring and logging
• Integrity checks to help ensure the product has not been altered.

The certified controller builds on the 2018 certification of the Rockwell Automation Security Development Lifecycle (SDL) to the IEC 62443-4-1 standard. Rockwell Automation uses the SDL at all its global development locations to develop secure hardware and software products for connected operations.

For more information on how to improve industrial control system security, visit.

About Rockwell Automation

Rockwell Automation Inc. (NYSE: ROK), the world’s largest company dedicated to industrial automation and information, makes its customers more productive and the world more sustainable. Headquartered in Milwaukee, Wis., Rockwell Automation employs approximately 22,000 people serving customers in more than 80 countries.

Media Contacts

Tom Spencer
Elena Gardiner

Latest News

Rockwell Automation and our partners offer exceptional knowledge to help design, implement, and support your automation investment.

Subscribe

Subscribe to Rockwell Automation and receive the latest news and information directly to your inbox.