THE MACHINE BUILDERS RESOURCES

Innovative thinking. Innovative machinery.

End-users want you to deliver smart machines and equipment that easily integrate into their facilities, provide access to pertinent, actionable information, and deliver the agility they need to react to changing market demands.

These examples show how we listen to their needs to help them to address these challenges, while working hard to help them save money, increase productivity, improve safety, and reduce downtime.

Filter & Refine

3V Automation Journeys to Digital Transformation

To position automakers for greater success, 3V Automation worked with Rockwell Automation to implement the latest digital technologies for smart machines and equipment.

Packaging Machine Builder Reduces Engineering Time

Bosch Packaging, a global leader in providing packaging solutions in food and pharmaceutical segment, reduces the time required for machine manufacturing.

KS PULSE Keeps It Simple in Latest Release

Faster, easier integration is now possible in this revolutionary approach to auto body assembly based on independent cart technology.

Sinhyung Reduces Commissioning Time

Sinhyung Engineering selected a single controls supplier to help meet the changing demands of its end users and create flexible, scalable machines.

Deyu Lights Up Efficient Battery Production

Deyu's winding machines help customers achieve higher productivity and lower cost in battery production, and enhance the reliability and energy density.

Large-scale Integrated PM Motor Control Solution

AT Equipment and Services GmbH, was tasked with the development of a precision control solution for two large permanent-magnet (PM) motors deployed in a dual-chamber shredding unit.

iTRAK Addresses Throughput Challenges

ECONO-PAK was approached by Lotte Wedel to develop a packaging/cartoner machine that would more easily cater for varieties in packaging formats and product counts.

Smart Machine Helps Ease Safety Compliance

Yalong’s gearbox assembly machine meets standard requirements for integrated safety, ultimately helping end users ease compliance and reduce costs.

System Conserves Space, Improves Load Stability

The Columbia Machine FL6200SW combines high-speed stretch wrap technology with a contemporary, modular and clean-design palletizer.

Rockwell Automation Improves Hydraulic System

Thanks to Rockwell Automation servo drives and AC drives, Neotecman has reduced the design, installation and setup time of its hydraulic stamping equipment.

Integrated Architecture Reduces Costs and Time

A global manufacturer of specialty papers and fibre-based engineered materials, wanted a new machine to connect seamlessly with a plant’s existing infrastructure.

Improving Productivity and Footprint with iTRAK

With variable pitch, higher speed and greater throughput forming the crux of a new assembly machine, Maga Active turned to Rockwell Automation with its innovative iTRAK® technology.

Hiperbaric Machines Get a Connectivity Boost

Enabled by EtherNet/IP network, the ControlLogix system helps perform remote management and maintenance tasks.

Oil and Gas: Thinking Outside the Black Box

Energy Control Technologies abandoned proprietary technologies in favor of an open-systems approach for a new turbomachinery process control solution.

OEM Solution: Newfoil Machines Limited

Newfoil Machines Limited has become world leader in the field of roll fed hot foil label printing and converting machines and can boast over 1,500 installations in 90 countries worldwide.

Cosma Brings The Connected Enterprise To Life

Italian machine builder engineers a new, high performing and completely connected line for washing machine chassis production.

Pulsar Deploys FactoryTalk Software to Measure OEE

Italian firm developed a platform for SCADA systems specifically for measuring overall equipment effectiveness in the tissue converting industry.

Thurne Brings Home the Bacon Using Advanced Vision

Bacon slicing accuracy is critical in order to help ensure consistency. Thurne-Middleby Ltd. opted for a solution that paired a precision vision solution with accurate control.

Compac Sorting Equipment Stays Ahead

Compac Sorting Equipment remains competitive and improves productivity by reducing time and costs associated with engineering disparate machine components.

OEM Solution: Columbia Machine

Designed for non-stop operations, this high-speed palletizer is built for optimal performance, safety and flexibility.

Simple Line Integration Slashed Costs

A major consumer supplier automated its reporting process, increased plant visibility and cut expenses by enabling repeatable integration.

OEM Solution: Premier Tech Systems

Completely automatic machine saves space while palletizing up to 50 cases per minute.

OEM Solution: Trinamics

Integrated cartoner/case packer is built to withstand rugged environment - and improve machine safety and availability on chicken processing line.

OEM Solution: DJS Systems

New control system enables 20% speed improvement on servo cup counter and vertical bagger system for the disposable foodservice industry.

OEM Solution: Jomar

Updated control system helps OEM save up to 30 minutes per changeover on injection blow molding equipment.

OEM Solution: Power Automation Systems (PAS)

New or existing facilities can take advantage of these innovative automated warehouse solutions to dramatically improve density and throughput.

OEM Solution: Roeslein

Innovative modular approach speeds design and delivery of aluminum can manufacturing systems.

OEM Solution: Bevcorp

For craft beverage producers and contract packagers, this cost-effective bottle filler makes high-volume rotary filling a viable option.

OEM Solution: MGS Machine

Efficient and serialization-friendly, this continuous motion cartoner meets pharmaceutical niche for bottle, tube or blister applications.

OEM Solution: Precision PMD

Versatile. Energy efficient. Take a look at this servo-driven denester for food packaging.

OEM Solution: Accraply

These space-saving machines speed changeover for roll-fed labeling and shrink-sleeve labeling applications.

OEM Solution: American Packaging Machinery (APM)

This cost-effective shrink-wrapping system for disposable dinnerware delivers a consistent and attractive shelf-ready package.

OEM Solution: Autotec Engineering

In-mold labeling equipment provides plastic processors with energy-efficient solution that meets exacting end-user requirements.

OEM Solution: Drake

For sausage, cheese sticks and other cylindrical food, make this autoloader part of your packaging line.

OEM Solution: Marchant Schmidt

Innovative cheese converting solution helps reduce "giveaway" and can significantly impact a food producer's bottom line.

OEM Solution: Product Handling Concepts

Convert your manual cleaning wipes packaging application to an automated system with this canister loader.

OEM Solution: Weiler Labeling System

For high-speed serialization applications, this pressure sensitive label head can deliver new levels of efficiency and flexibility.

OEM Solution: Combi Packaging Systems

The Ergopack hand packing station offers a robot-assisted option to minimize human intervention in difficult or hazardous packing tasks.

OEM Solution: AFA Systems

Integrated cartoner and robotic case packer optimizes changeover time - and energy efficiency on powdered milk packaging line.

OEM Solution: C&M Conveyor

Computer inventory management system (CIMS) coordinates plant-wide material delivery completely automatically or semi-automatically.

OEM Solution: Forpak

Ideal for larger food products, such as pizza, this stacker helps ensure the right count at a rate of 80 pieces per minute.

OEM Solution: TechniBlend

Automated blending system delivers new level of efficiency and flexibility to carbonated beverage plants.

Highly Capable and Cost Effective Tray Erector

Linkx Systems Ltd. creates highly capable and cost effective entry-level tray erector to save space and cost without compromising on performance.

Return on Investment by Zipper Packaging

The Newton TX flexible packaging machine, created by UVA Packaging, packages stand-up pouches, especially those which are also resealable.

Increased Productivity in Food Washing Machinery

Italian machine builder, Turatti, delivers higher productivity and seamless data distribution thanks to the PlantPAx™ Process Automation System from Rockwell Automation

ALD Deploys Integrated Control Solution

Vacuum technology company deploys integrated, single-platform, Logix-based solution for the control of automation, safety, process and motion.

Bradman Lake Demonstrates Control Platform

Leading packaging technology company deploys Rockwell Automation solutions across its range, resulting in significantly reduced engineering effort and greater interoperability

Kliklok-Woodman Create Packaging Solultion

Rockwell Automation Motion Analyzer and Dassault Systèmes SolidWorks software partnership create a new improved packaging solution.