Driving Paper Production at Visy’s Pulp and Paper Mill

Driving Paper Production at Visy’s Paper Mill

Challenge

  • To engineer, commission and install a winder control and drive system upgrade at Visy’s Tumut plant

Solutions

Results

  • Hassle-free Commissioning – Commissioning was conducted within a planned shutdown with no issues; First roll produced by the paper machine was sellable quality
  • Local Service and Support – Remote access helps with troubleshooting; Local service and support is available as required

Paper Machine 9 Winder upgrade future-proofs paper production

Visy is a global leader in the packaging, paper and resource recovery industries, providing high quality, innovative and sustainable packaging products and solutions.

The company has been leading packaging innovation in Australia for over 60 years and has more than 120 sites across Australia, New Zealand, Thailand and Vietnam and trading offices across Asia, Europe and the USA.

Sustainability is a pillar of Visy’s business. From the products they make, to resource recovery cycles and the business, including making employees safer, local communities healthier and customers more profitable.

Limiting impact on the environment is one of Visy’s key missions. They take responsibility for the entire lifespan of their products - from conception to when they are recycled into something else.

Visy’s Pulp and Paper mill in Tumut, New South Wales is the largest integrated pulp and paper mill in Australia and has set new standards in sustainable kraft paper manufacturing and environmental performance - producing high-quality kraft paper for both domestic and international markets.

Two million tonnes of plantation-sourced wood is processed at Tumut each year, meaning that a wood truck arrives at the site every five minutes, each day. The site is one of Australia’s largest exporters of containerised manufactured goods and hosts a renewable energy generation facility, producing half of the plants own energy needs. Visy Tumut also operate a closed loop water system, where all mill wastewater is reused for farm irrigation.

In FY2017-18, Paper Machines 9 (PM9) and 10 (PM10) at VISY Tumut produced over 681,000 tonnes of unbleached kraft paper.

As a company that is always looking towards the future, Visy took a proactive approach in upgrading legacy drive control equipment on the PM9 winder downstream of the paper machine to avoid any potential for downtime while also future proofing the Tumut plant.

Planning and design

Visy contracted Rockwell Automation to conduct the planning and design stage of the project.

The Allen-Bradley® PowerFlex® 755TM drive system provided a small footprint with motoring and regenerating capabilities.

Matthew Barrett, senior project engineer, Rockwell Automation, explained that, “The first step of the project was to perform a Front End Engineering Design (FEED) study. As part of this process we worked closely with Visy to gain a detailed understanding of the engineering requirements for the winder upgrade.” Upon completion of the FEED, a detailed proposal was prepared and the upgrade commenced.

Visy’s Tumut plant produces high quality linerboard paper for cardboard boxes. Paper Machine 9 produces a ‘jumbo roll’ that is 3.2m in diameter by approximately 5.5m wide. This jumbo roll then moves into the winder, which cuts the paper into smaller rolls to suit customer requirements and allows for easy shipping. Each roll coming off the winder is wound with a specific tension profile, to avoid collapse or telescoping.

Latest drive technology

The operational requirements of the drive system are very demanding — it must be able to rapidly accelerate and decelerate the heavy rolls and maintain web tension and production speed of up to 2500 metres/minute while the diameters of the rolls are changing.

The paper machine produces a ‘jumbo roll’ that is 3.2m in diameter by approximately 5.5m long.

To achieve consistent roll quality, it is essential to keep the whole winder system stable. Settings on the drives and control system must be finely tuned to ensure that tension fluctuations do not affect the roll structure. To achieve this, coordination of the drives on the winder was crucial. “If all the drives are not coordinated, the winder is unable to work effectively,” explained Barrett.

The latest generation of drives from Rockwell Automation, the Allen-Bradley® PowerFlex® 755TM drive system was the best choice for this application. These drives were designed to provide harmonic mitigation, regeneration and common bus solutions that help reduce energy costs, add flexibility and increase productivity.

The coordinated drive systems reduce energy consumption as they are able to share energy on the bus — some drives are motoring while others are regenerating. With a smaller footprint than the legacy system, the drives were able to reduce the space required to house the system.

Control requirements were provided by Allen-Bradley GuardLogix® controllers and all safety devices were upgraded to CAT3, Pld. Further safety upgrades are easily achievable due to the GuardLogix system being installed. Ethernet/IP™ provided secure communications between the controller and drives.

The jumbo roll then moves into the winder, which cuts the paper into smaller rolls.

HMI requirements for the winder were delivered by FactoryTalk® View software. The WindPro solution was engineered by Rockwell Automation to help paper manufacturers monitor and control paper roll density and help prevent quality defects, such as wrinkles and tears. It provides real-time winder control and monitoring including recipe management, roll data, general operator interface to the winder, faults, alarms and trending.

Barrett explained that, “This was one of the first applications in the world that used the new PowerFlex 755TM drives so we worked closely with the product specialists in the US regarding some of the technical aspects of the drives.”

“As there was a limited time available for commissioning the new system, we conducted a Factory Acceptance Test (FAT) to provide a complete simulation of the machine. This allowed Visy to see the drive system in operation and we were able to go through all of the functions to make sure it met Visy’s requirements,” he said.

The installation and commissioning of the system was conducted during the plant’s annual shutdown, with no significant issues. In fact, the first roll produced by the winder was sellable quality.

Remote access with local service and support

 “The new winder drive system is working well and there has been no downtime due to drive system issues. We have remote access to the system which helps with troubleshooting as required,” said Barrett.

Thanks to local service and support from Rockwell Automation, Paper Machine 9 at Visy’s Tumut plant can continue to produce high quality kraft paper for Australia and the world.

“The technical support from Rockwell Automation has been great. The new control and drive system for the winder is performing really well and by having remote access to the system, Rockwell Automation is able to continue to provide support as required. The project has been a success for Visy and we are very confident in the Rockwell Automation team,” said Santiago Vargas, Visy Tumut project engineer.

Allen-Bradley, FactoryTalk, GuardLogix, PowerFlex, Rockwell Automation and Rockwell Software are trademarks of Rockwell Automation, Inc.

EtherNet/IP is a trademark of ODVA, Inc.

Blog

We want to keep you up to date with what is happening in your industry to help you get ahead in the future. The Rockwell Automation Blog is a platform for our employees and guest bloggers to share technology and industry-related topics.