Set Up a Redundant Chassis Pair

The setup process of a redundant chassis pair consists of the following:
  • Firmware bundle installation
  • FactoryTalk® Linx
    Redundancy Module Configuration Tool (RMCT) installation
  • Redundant chassis component installation and firmware updates
  • Identification of the primary and secondary chassis
  • Qualification and synchronization verification
After setup, you can reset, remove, and replace redundancy modules as needed.

Before You Begin

Before you begin, do the following:
  • Make sure that the redundant chassis pair has the required matching components. For best performance, place the redundancy module in the chassis as close as possible to the controller.
  • Read and understand the safety and environmental considerations explained in the installation instructions for each component.
  • Download and install the compatible versions of the
    Studio 5000 Logix Designer®
    application, communication software, and
    ControlFLASH Plus®
    software. For information on how to download and install
    ControlFLASH Plus®
    software, see the ControlFLASH Plus Quick Start Guide, publication CFP-QS001.
    IMPORTANT: If communication software is already on your system, be sure to shut it down before you install or update software.
  • Review the release notes for the firmware bundle that you are installing. Make sure that you have compatible hardware and the correct firmware revisions.
  • Determine the IP address for each of your Ethernet/IP™ communication modules. Both communication modules in the redundant chassis pair usually have the same IP address. See IP Address Swapping.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal