Create a client panel loader

Create a panel loader that will fetch panel data from the Server project.
  1. In
    Project view
    , right-click
    MainWindow (type)
    and select
    New
    Containers
    Panel loader
    .
  2. Hover-over the panel loader, select
    Edit
    , and enter
    ClientPanelLoader
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.