Configure idle Timeout for a session

Use the UI Session
IdleTimeoutEvent
to have an idle timeout apply to the entire session and the Presentation Engine.
  1. In
    Project view
    , right-click the
    UI
    folder and select
    New
    UI Session
    .
    UISession# (type)
    appears in
    Project view
    .
  2. With
    UISession# (type)
    selected, in
    Properties
    , in
    Inactivity timeout duration
    , enter the duration for the timeout.
  3. In
    Inactivity timeout active
    , select
    True
    .
  4. Under
    Events
    after
    IdleTimeoutEvent
    , select
    Add
    Add new method
    , expand
    Commands
    , and navigate to select the command that will be executed when the timeout event is triggered.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal