PolyLine

PolyLine that can be adapted to fit the design needs.
BrowseName
PolyLine
SuperType
Container(Container)

Properties

Name
BrowseName
DataType
Description
Border color
LineColor
Color of the polygon border.
Fill color
FillColor
Fill color of the polygon area.
Thickness
LineThickness
Line thickness.
Blink
Blink
Allows the object to periodically blink, ignored when the object is not visible.
Path
Path
Path.
Hit test visible
HitTestVisible
True = intercept user clicks. False = does not intercept user clicks, which are instead passed to the underlying object, based on the order on the Z axis.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)

Events

MouseDown event
BrowseName
MouseUp event
BrowseName
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.