LED

Display a Boolean value as an LED that is on or off.
BrowseName
Led
SuperType
Element(Item)

Properties

Name
BrowseName
DataType
Description
Text
Text
Text to be displayed.
Appearance
Appearance
LED appearance.
Color
Color
Color of the pen line.
Active
Active
LED status.
Blink when active
BlinkWhenActive
Enable/disable blinking when Active = True.
Image path
ImagePath
Icon to be displayed in the navigation tab of a Navigation panel object.
Image position
ImagePosition
Position of the image to display.
Text position
TextPosition
Position of the text on the horizontal and vertical axes relative to the sides of the object.
Image width
ImageWidth
Width of the image to display. The Auto value sets the native width of the image.
Image height
ImageHeight
Height of the image to display. The Auto value sets the native height of the image.
Word wrap
WordWrap
Enable/disable the automatic word wrapping when the text is wider than the container. Ignored when the object width is automatic or when text abbreviation is set.
Text trimming
Elide
Text trimming mode. Insert three dots (...) in the indicated position when the text is too long for the available space. Ignored when the object width is automatic or when word wrap is set.
Font family
FontFamily
Font family.
Font weight
FontWeight
Font weight.
Font italic
FontItalic
Enables/disables italics in the text.
Font size
FontSize
Font size.
Text color
TextColor
Color of the text to display.
Visible
Visible
(Inherited from Element)
Enabled
Enabled
(Inherited from Element)
Opacity
Opacity
(Inherited from Element)
Left margin
LeftMargin
(Inherited from Element)
Top margin
TopMargin
(Inherited from Element)
Right margin
RightMargin
(Inherited from Element)
Bottom margin
BottomMargin
(Inherited from Element)
Width
Width
(Inherited from Element)
Height
Height
(Inherited from Element)
Horizontal alignment
HorizontalAlignment
(Inherited from Element)
Vertical alignment
VerticalAlignment
(Inherited from Element)
Rotation
Rotation
(Inherited from Element)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.