Register an Extractor

To run data transformation using Auth0 as the IdP, CDF requires client credentials (M2M Token). To get the appropriate client credentials, you must first register an extractor and save the client ID and secret generated.
Perform the following steps to register an extractor:
  1. On the FactoryTalk DataMosaix Management Console, select the
    Extractor Info
    tab.
  2. Click the Add [+] icon.
  3. On the Extractor Info Detail page, provide a unique and meaningful name for the extractor.
  4. In the Pipeline field, provide the extraction pipeline name created earlier.
  5. Select the
    Source Type
    as Add Custom / Other.
    Extractor Info Detail Page
  6. Click
    Save and Apply
    to register the extractor. Credentials and other information are displayed.
  7. Copy and save the client secret information. You will need to use this information while setting credentials to run data transformation.
    Credentials and Other Info
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal