In this video, Adam Lindsey from Rockwell Automation Encompass™ Product Partner Spectrum Controls Inc. describes the company's BACNet module for the Allen-Bradley® Micro800® controller platform from Rockwell Automation.
Also see Spectrum's new I/O cards for the 1734 POINT I/O™, including a popular two-channel HART analog output module; the new full-color InView industrial message displays; and the new features for improved functionality on the Spectrum WebPort industrial remote access solution, an industrial gateway that lets users access controllers from anywhere by using Ethernet or cell phone.
Watch the video now!