In this video from the 2018 Automation Fair® event, Vernon Gross from Det-Tronics explains the Eagle Quantum Premier (EQP) control flame and gas safety controller with DLR outputs, a SIL-2 capable, fault-tolerant, addressable system to detect fire and gas. The DLR protocol provides direct communication to Allen-Bradley® PLCs.
Unique features: 1) globally certified to the latest standards for fire and gas safety system performance and hazardous locations, and 2) the large amount of data provided to the operator on its screen.
Click the image above to view the video.
The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.