In this video, Eugene Detke from Apex Dynamics, Inc. demonstrates the company’s new AF series, a carbon steel, planetary gear box with high precision, quiet operation, and ≤1arcmin in a single stage, plus double stages and larger sizes for bigger applications.
Also see Apex’s expanded rack-and-pinion line with quality 6C carbon steel and milled versions, and rack-and-pinion lubrication system with grease- or oil-filled lubrication for up to 16 points of lubrication.
Click the image above to watch the video and see the technology in action.
The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.