Change the EtherNet/IP Mode in FactoryTalk Linx Software
This example shows the
EtherNet/IP™
mode change from Dual-IP mode to Linear/DLR mode. The same tasks apply to change from Linear/DLR mode to Dual-IP mode.
IMPORTANT:
With
ControlLogix®
5590 controllers, the Ethernet ports on the controller itself are labeled 1 and 2. In programming and communication software, the ports are described as A1 and A2.Make sure that you are aware of the effects of changing the
EtherNet/IP™
mode. See Change the EtherNet/IP Mode.- Confirm that the controller is online and there is no project in the controller.
- Confirm that the controller is in one of the following modes:
- Program
- Remote Program
- Remote Run
You cannot change theEtherNet/IP™mode if the controller is in Run mode. - Right-click the controller and choose Device Configuration.

- From the dropdown menu on the IP Mode tab, choose the new mode.

- When theEtherNet/IP™Mode Change warning appears, read it carefully, and click Yes.

Provide Feedback