I/O Module Properties
The Module Properties dialog box for an I/O device shows fault information, such as:
- Module state
- Fault description
- Major and minor fault descriptions
- Module's internal state
- Diagnostics information
Module Status on General Category
The General category shows a Faulted status.
I/O Fault Status on Overview Category

Module Fault Description on Connection Category
The Connection category displays the module fault description that includes an error code that is associated with the specific fault type.
I/O fault on Connection Category

Module Fault Descriptions on Module Info Category
The Module Info view requires successful communication.
- If communication to the I/O module is OK, but the module itself is faulted, then the Module Info tab helps to troubleshoot the fault.
- If there is a communication fault, then the Connection Tab is more useful.
On the Module Info category, the Status section displays the following about the I/O module:
- Major and Minor Faults
- Internal State
I/O Fault on Device Information View

Provide Feedback