Controller Diagnostics with Linx-based Software

You can also view diagnostic information in Linx-based software.
  1. From the Communications menu, select Who Active or Network Browser.
  2. Navigate to the controller on the
    EtherNet/IP
    network.
    This image shows where to browse to a GuardLogix 5580 controller on Who Active.
  3. Right-click the controller and choose Device Statistics.
The Statistics dialog box shows a variety of information.
This image shows module statistics in Logix Designer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal