I/O Device Address Format

When you add a device to the I/O configuration, the
Studio 5000 Logix Designer®
application creates controller-scoped tags for the device.
I/O information is presented as a set of tags. Each tag uses a structure of data, depending on the type and features of the I/O device. The name of a tag is based on the name of the device.
A safety I/O device address follows this example:
devicename:Type.Member
Safety I/O Device Address Format
Where
Is
device name
The name of the safety I/O device.
Type
Type of data
Input: I
Output: O
Membership
Specific data from the I/O device
Input-only device
devicename:I.RunMode (required)
devicename:I.ConnectionFaulted (required)
devicename:I.Input Members
Output-only device
devicename:I.RunMode (required)
devicename:I.ConnectionFaulted (required)
devicename:O.Output Members
Combination I/O
devicename:I.RunMode (required)
devicename:I.ConnectionFaulted (required)
devicename:I.Input Members
devicename:O.Output Members
For more information on addressing standard I/O devices, see the Logix 5000 Controllers I/O and Tag Data Programming Manual, publication 1756-PM004.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal