Change Configuration Ownership

When the controller project is online, the Safety tab of the device Properties dialog box displays the current configuration ownership: .
  • When the opened project owns the configuration, Local is displayed.
  • When a second device owns the configuration, Remote is displayed, along with the SNN and the node address or slot number of the configuration owner.
  • If the device read fails, a communication error appears
If the connection is Local, you must inhibit the device connection before resetting ownership. Follow these steps to inhibit the device.
  1. Right-click the device and choose Properties.
  2. Click the Connection tab.
  3. Check Inhibit Connection.
  4. Click Apply and then OK.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal