History of Changes
1756-UM543S-EN-P, November 2025
Topic |
|---|
Added content to the ATTENTION table in section Protect the Safety Signature |
Updated the User Initiated row in the Controller Power table that explains how what happens when you insert a memory card and powerup the controller |
Moved topic Trusted Slots Slots on the Controller to chapter Manage Controller Communications |
Updated content in the ATTENTION table in section Develop Safety Applications |
Added topic CIP Bridging Control to chapter Develop Secure Applications |
Added content on how to access diagnostic assembly information |
1756-UM543R-EN-P, December 2024
Change |
|---|
Updated Additional Resources table |
Revised Controller Redundancy section |
Revised Secure Controller Systems section |
Added IEC-62443-4-2 SL 1 security certification content for safety controllers |
Added statement about impact of license-based source protection on download times |
Added Privacy Aspects section |
Added information about unique code for troubleshooting major faults Type 1, Codes 60, 61, 62 |
1756-UM543Q-EN-P, July 2024
Change |
|---|
Updated information about system compatibility and extreme environment ratings |
Added catalog numbers 1756-L81ESXT, 1756-L82ESXT, 1756-L83ESXT, 1756-L84ESXT, 1756-L8SPXT, 1756‑L81E‑NSEXT, 1756-L82E-NSEXT, 1756-L83E-NSEXT, 1756-L84E-NSEXT, 1756-L85E-NSEXT, 1756-L81EPXT, 1756‑L83EPXT, and 1756-L85EPXT |
Updated information about conformal coated products |
Added recommended SD cards |
1756-UM543P-EN-P, November 2023
Change |
|---|
Added catalog number 1756-L85ES |
Revised the Safety Signature section in Chapter 2 |
Updated the controller Safety tab screenshots |
Updated the Safety I/O Replacements Options section |
Added a statement about the status of the Enable Controller Webpages checkbox |
1756-UM543O-EN-P, February 2023
Change |
|---|
Updated the controller minimum requirements |
1756-UM543N-EN-P, November 2022
Change |
|---|
Moved information about connection reaction time limit to publication 1756-RM012 |
Added GuardLogix-XT™ catalog numbers |
Revised ControlLogix-XT™ and GuardLogix-XT™ Controllers section |
Revised information about the safety signature |
Added 1756-EN4TR, 1756-EN4TRK, 1756-EN4TRXT catalog numbers |
Added information about secure socket objects |
Added introduction and Program Safety Applications section to Chapter 11 and moved other safety topics from Chapter 11 to publication 1756-RM012 |
Added information about component tracking |
1756-UM543M-EN-P, May 2022
Change |
|---|
Added publication to the Additional Resources table |
Separated ControlLogix® and GuardLogix® K catalog numbers |
Updated CIP Security™ content |
Added CIP Security™ to ControlLogix® and GuardLogix® controller feature tables |
Added CIP Security™ considerations for the number of EtherNet/IP™ nodes |
Added K controllers to the description of ControlLogix® 5580 controllers that support |
IEC-62443-4-2 SL 1 security requirements |
Added syslog collector to controller system image |
Restructured security checklists |
Moved Verification of Security Implementation content to the beginning of security checklist |
Changed “ Studio 5000 Logix Designer® application” checklist item in Table 37 from “yes” to “may be required” for IEC-62443-4-2 SL 1 security requirements |
Added FactoryTalk® Security software to Table 38 and revised details |
Revised details of “Firmware update” checklist item in Table 38 |
Added “Syslog collector” checklist item to Table 41 |
Changed “Controller log” checklist item in Table 41 to “Disabled controller log auto-write” and revised details |
Added information about matching firmware revisions and Trusted® slots |
Changed NVS to non-volatile controller memory |
Added syslog log collector to Controller Log section |
Added method to disable CIP Security™ ports in FactoryTalk® Linx software |
Updated general status messages for the controller |
1756-UM543L-EN-P, August 2021
Change |
|---|
Updated link to Logix Controller and I/O Fault Codes |
Updated Conformal Coated Products statement |
Updated Controller Log section |
Added Controller Status messages |
1756-UM543K-EN-P, August 2020
Change |
|---|
Added ControlLogix® NSE, ControlLogix-XT™ , and ControlLogix® Process controllers |
Updated safety signature definition |
Updated behavior of controller status indicators while loading a project from the SD card |
Added Simple Network Management Protocol (SNMP). |
Added Automatic Diagnostics |
Added Considerations for Communication Loss Diagnostics |
1756-UM543J-EN-P, October 2019
Change |
|---|
Added links to access Controller and I/O fault code information from the Knowledgebase Support Center |
1756-UM543I-EN-P, March 2019
Change |
|---|
Moved information on Controller and I/O fault codes to the attached spreadsheets |
Added Develop Secure Applications chapter |
Updated Controller webpage information |
1756-UM543H-EN-P, August 2018
Change |
|---|
Updated the ControlLogix® and ControlLogix-XT™ Chassis and Slots table |
1756-UM543G-EN-P, July 2018
Change |
|---|
Changed some remaining instances of “safety task signature” to “safety signature” throughout |
Updated the Assign the Safety Network Number (SNN) section |
Updated the Copy and Paste a Safety Controller Safety Network Number section |
Updated the Set the SNN of a Safety I/O Device section |
1756-UM543F-EN-P, February 2018
Change |
|---|
Added GuardLogix® 550 controllers and Safety Information |
1756-UM543E-EN-P, December 2016
Change |
|---|
Updated tables with new maximum number of EtherNet/IP™ nodes that are supported in Version 30 or later |
Added the 1756-IF16IH module to the list of supported HART devices |
1756-UM543D-EN-P, August 2016
Change |
|---|
Added the catalog numbers 1756-L81E, 1756-L82E, 1756-L84E |
Added ControlFLASH™ to the Required Software section |
Added the section ‘ EtherNet/IP™ Network Communication Rates' |
Added information on the Ethernet node counter to the section 'Nodes on an EtherNet/IP™ Network |
Added the appendix ‘Security Options’ |
1756-UM543C-EN-P, November 2015
Change |
|---|
Updated the diagram for multiple controllers in one chassis |
Provide Feedback