Requirements for Data Confidentiality
Security Component | Required to Meet IEC‑62443-4-2 SL 1 | Details |
|---|---|---|
FactoryTalk® Security software | Yes | Configure FactoryTalk® Security to define policies, user groups, and other permission sets.
For more information, see Configure System Security Features User Manual, SECURE-UM001 . |
FactoryTalk® Policy Manager software | Yes | Use the FactoryTalk® Policy Manager software to define a secure data transport over an EtherNet/IP™ network to the controller.For more information, see Configure System Security Features User Manual, SECURE-UM001 . |
License-based source and execution protection | May be required based on system design, threat model, and risk assessment. | Configure licenses to manage access to controller source logic and execution of that logic. These licenses are not enabled by default.
For more information, see License-based Source and Execution Protection. |
Access to tag data | May be required based on system design, threat model, and risk assessment. | Configure the following attributes in the Logix Designer application to control access to tag data:
|
Provide Feedback