Methods to Set the IP Address
The controller supports the following methods to change the IP address:
- BootP/DHCP EtherNet/IP Commissioning Tool
- FactoryTalk® Linxsoftware
- Studio 5000 Logix Designer®application
For more information on how to use these methods, see the
EtherNet/IP™
Network Device User Manual, publication ENET-UM006.Provide Feedback