Create Tag Mapping Pairs

  1. From the Logic menu, select Map Safety Tags.
    Safety Tag Mapping Dialog Box
  2. In the Standard Tag Name or Safety Tag Name column, enter or select an existing tag:
    • To show only controller-scoped standard tags, click the arrow in the Standard Tag Name column.
    • To show only controller-scoped safety tags, click the arrow in the Safety Tag Name column.
    Filter Tag Names
  3. In the Standard Tag Name or Safety Tag Name column, add a new tag:
    1. Right-click in the empty cell.
    2. Select New Tag.
    3. Enter the tag name into the field.
  4. Right-click the field and select New tagname, where tagname is the text you entered in the field.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal