View alarm quality
View the quality of alarms which is detected through controller faults. While there can be several faults or reasons that determine the quality of an alarm, each alarm is assigned only one quality -- good, bad, or uncertain. If there is no fault, the quality of the alarm quality is good. If the status of a controller status is not read yet, the quality of the alarm is uncertain.
To view alarm quality
- Open theAlarm Managerscreen.
- Select to select the alarm. Using an external keyboard, tab to highlight the alarm list and press theUp ArroworDown Arrowto select the alarm.
- In theDetailspane at the bottom of the Alarm Manager table, select the horizontal scroll arrows to scroll to theQuality Detailrow. This row lists the quality of the alarm. The quality of the alarm is bad if the alarm has one of these faults:
- Instruct fault only (specific fault not set)
- Instruction faulted
- Severity invalid
- Alarm limits invalid
- Deadband invalid
- ROC positive limit invalid
- ROC negative limit invalid
- ROC period invalid
- Old Logix firmwareTIP:If an alarm has a fault, aBad Quality
icon appears in the Inhibit Statecolumn of the Alarm Manager table.
Provide Feedback