View alarm errors
Performing an operation that fails for an alarm, such as disabling an already disabled alarm, shows an
on the alarm table. Alarm operation errors are write errors. The
Error
icon
on the alarm table. Alarm operation errors are write errors. The Error
icon disappears after 10 seconds. Unlike read errors, the error does not keep displaying the Error
icon. An Error
icon opens an Error list
that contains:- The affected alarm table -- Alarm Summary or Alarm Manager
- The alarm
- The condition triggering the alarm
- A description of the error
To view alarm errors
- Open theAlarm Summaryscreen or theAlarm Managerscreen.
- In the alarm table, select alarms:
- Perform the operation. If an error occurs for the operation, an
- Individual alarm.Tap to select the alarm. Using an external keyboard,Tabto highlight the alarm list. Select theUp ArrowandDown Arrowto select alarms in the list.
- Page of alarms.To select all alarms visible on the current page of alarms, selectSelect Page

- All alarms.To select all alarms, including those not visible on the current page of alarms, selectSelect All

Erroricon
appears in the upper left corner of the alarm table. - Select theErroricon
. The list of alarms in the alarm table turns red and an Error listappears. When multiple alarms or conditions are in error, multiple error messages in theError list.TIP:Disabled buttons have diagonal hash marks. Selecting a disabled button shows anErroricon
on the button for 10 seconds. Selecting the Erroricon
displays an Error listwith the message that the button is disabled.
Provide Feedback