View alarm details
View alarm details to display more information about an alarm. Additional details appear for alarms in the
Alarm Summary
and Alarm Manager
. Details include: - Alarm severity
- Associated tag values
- Alarm message
- The time an alarm entered a specific state
- Individual conditions for the alarm (Alarm Manager only)
To view alarm details
- Open theAlarm Summaryscreen or theAlarm Managerscreen.
- In the alarm table, select an alarm.
- SelectDetails
. A Detailspane with additional information for the last selected alarm opens at the bottom of the alarm table. TheDetailspane replaces medium alarm tables configured for six-inch to nine-inch HMI devices. Details show for an individual alarm condition in anAlarm Summary. - SelectDetails
to hide the details for the selected alarm.TIP:Tips:- To show details for an alarm condition in anAlarm Manager, select the condition in theDetailspane of the Alarm Manager table.
- Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
Provide Feedback