View alarm condition details
Display alarm condition details to view more information about an alarm condition. Additional details for an alarm condition appear in the
Details
pane of the Alarm Manager
table. To view alarm condition details
- Open theAlarm Managerscreen.
- Select the alarm.TIP:Using an external keyboard, pressTabto highlight the alarm and pressEnterto select the alarm.
- SelectDetails
. The Detailspane with additional information for the selected alarm appears at the bottom of the alarm table. TheDetailspane replaces the alarm table on medium HMI devices. - In the pane of individual alarm conditions to the left of theDetailspane of the Alarm Manager table, select the condition. The details of the alarm condition appear.
- SelectDetails
to hide the details for the selected alarm.TIP:Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
Provide Feedback