Unshelve an alarm
Unshelving an alarm allows notification of new state changes to the alarm. Unshelve an alarm from the
Alarm Manager
. Unshelve an alarm for a piece of equipment in a system that is no longer under maintenance. Unshelving an alarm unshelves all conditions for the alarm. Alarms unshelve automatically when the default shelving duration from the controller expires. To unshelve an alarm
- Open theAlarm Managerscreen.
- Select the alarms:
- Individual alarm.Tap to select the alarm. Using an external keyboard,Tabto highlight the alarm list. Select theUp ArrowandDown Arrowto select alarms in the list.
- Page of alarms.To select all alarms visible on the current page of alarms, selectSelect Page

- All alarms.To select all alarms, including those not visible on the current page of alarms, selectSelect All

- At the bottom of the Alarm Manager table, selectUnshelve
. Notification of new state changes to the alarm occur. TIP:Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
Provide Feedback