Unshelve an alarm condition
Unshelving an alarm condition allows notification of new state changes to the condition. Unshelve individual alarm conditions from an Alarm Manager table. Alarm conditions are unshelved automatically when the default shelving duration configured for the controller expires.
To unshelve an alarm condition
- Open theAlarm Managerscreen.
- Select the alarm.TIP:Using an external keyboard, pressTabto highlight the alarm list. Press theUp ArrowandDown Arrowto select the alarm in the list.
- At the bottom of the Alarm Manager table, selectDetails
. The Detailspane appears at the bottom of a large Alarm Manager table or replaces a medium Alarm Manager table. Details appear for the last selected alarm. - To the left of theDetailspane, select the condition to unshelve, such as HIHI.
- On a large Alarm Manager table, selectUnshelve
above the condition list on the left side of the Detailspane. On a medium Alarm Manager table, selectUnshelve
below the Detailspane. Only the selected alarm condition is unshelved.The state of the condition is indicated in theInhibit State rowof theDetailspane. It is also indicated in theInhibit Statecolumn for the alarm in the Alarm Manager table.TIP:Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
Provide Feedback