Shelve an alarm condition
Shelving an alarm condition prevents the notification of new state changes to the condition. Shelve an alarm condition from the Alarm Manager table. Shelving an alarm condition shelves only that condition. The alarm condition remains shelved until the shelve duration from the controller expires automatically or when unshelving the alarm condition manually.
To shelve an alarm condition
- Open theAlarm Managerscreen.
- Select the alarm. Using an external keyboard, pressTabto highlight the alarm list. Press theUp ArrowandDown Arrowto select the alarm in the list.
- At the bottom of the Alarm Manager table, selectDetails
. The Detailspane appears at the bottom of the Alarm Manager table, or replaces the alarm table on medium HMI devices. Details appear for the last selected alarm. - To the left of theDetailspane, select the condition to shelve. For example, select HIHI.
- Above the condition list on the left side of theDetailspane, selectShelve
to shelve the selected alarm condition.TIP:Tips:- The state of the condition is indicated in theInhibit Staterow of theDetailspane. AShelvedicon appears in theInhibit Statecolumn for the alarm in the Alarm Manager table.
- Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
- The HMI designer may useLogix Designerto change the Shelve Duration and Max Shelve Duration. If the HMI designer does not change the Shelve Duration and Max Shelve Duration values usingLogix Designer, the updated values do not propagate to the Alarm Summary and Alarm Manager clients. The table uses the previous Shelve Duration and Max Shelve Duration values when shelving alarms.
Provide Feedback