Select an alarm
Select alarms to perform an operation on one or more alarms. Select alarms to acknowledge, shelve, unshelve, disable, enable, or reset a latched alarm. Deselect alarms to not perform an operation on those alarms.
To select an alarm
- Open theAlarm Summaryscreen or theAlarm Managerscreen.
- In the alarm table, select the up and down arrows in the scroll bar, or drag the thumb between the scroll arrows to view the next or previous alarm.
- Select alarms to highlight rows:TIP:Tips:
- To deselect all alarms, selectDeselect All
. - Select only one alarm at a time. Selecting multiple alarms or dragging to select multiple alarms is not allowed. Selecting an alarm and selecting another alarm selects only the last selected alarm. Selecting all alarms or a page of alarms deselects the previous selection and applies the new selection to the table.
- If not all expected alarms show in an alarm table, in theFilterbox at the bottom of the alarm table, selectNo Filter.
- To select an alarm using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
Provide Feedback