Reset alarm counts
Alarm counts indicate the number of times an alarm enters the In Alarm State. Resetting alarm counts resets the alarm count in the controller to zero. It also resets the Count value in the
Details
pane of the alarm table to zero. Reset alarm counts to gauge how many additional times or how fast an alarm enters the In Alarm State. Resetting counts for an individual alarm condition in the Details
pane of the Alarm Manager table is not supported. Counts for all conditions for the selected alarm are reset.To reset alarm counts
- Open theAlarm Managerscreen.
- Select the alarm.TIP:Using an external keyboard, pressTabto highlight the alarm and pressEnterto select the alarm.
- At the bottom of the table, selectReset Alarm Counts
. The alarm count in the controller, and the Alarm Count value in the Detailspane of the Alarm Manager table are reset to zero.TIP:Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
Provide Feedback