Enable an alarm
Enabling an alarm effectively turns on the alarm. Enable any number of alarms selected in an Alarm Manager table. Enabling individual alarm conditions in the
Details
pane of the Alarm Manager table is not supported.To enable an alarm
- Open theAlarm Managerscreen.
- Select the alarms:
- Individual alarm.Tap to select the alarm. Using an external keyboard,Tabto highlight the alarm list. Select theUp ArrowandDown Arrowto select alarms in the list.
- Page of alarms.To select all alarms visible on the current page of alarms, selectSelect Page

- All alarms.To select all alarms, including those not visible on the current page of alarms, selectSelect All

- At the bottom of the Alarm Manager table, selectEnable
. The selected alarms are enabled.TIP:Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
Provide Feedback