Disable an alarm
Disable an alarm to not evaluate the alarm condition. This turns off the alarm. Disabling an unacknowledged alarm does not acknowledge the alarm. Disabling individual alarm conditions in the
Details
pane of an alarm table is not supported. The Alarm Manager
shows disabled alarms. The Alarm Summary
shows disabled alarms that are unacknowledged. To disable an alarm
- Open theAlarm Summaryscreen or theAlarm Managerscreen.
- On the alarm table, select the alarm to disable:
- At the bottom of the alarm table, select
- Individual alarm.Tap to select the alarm. Using an external keyboard,Tabto highlight the alarm list. Select theUp ArrowandDown Arrowto select alarms in the list.
- Page of alarms.To select all alarms visible on the current page of alarms, selectSelect Page

- All alarms.To select all alarms, including those not visible on the current page of alarms, selectSelect All

Disable
. The Disableicon appears in theInhibit Statecolumn for the alarm.TIP:Tips:- Using an external keyboard, tab to highlight a button on an alarm table and pressEnter.
- To prevent alarm notifications while continuing to log state changes, the HMI Designer may configure an alarm suppress in theLogix Designerproject in the controller.
Provide Feedback