Cancel the export of alarm history

Cancel the export of the alarm history to stop creating the export file for the alarm history and not save it to removable media. Cancel the export when the alarm history for the current project is exporting to the USB storage device or SD card in the HMI device.
To cancel the export of alarm history
  1. Open the
    Settings
    screen.
  2. Select
    Data Export
    . The
    Data Export
    popup opens, showing the progress of the export.
  3. Select
    Cancel
    . The progress indicator stops to indicate the export is cancelled.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal