Help popup
How do I open the Help popup?
- Open an alarm table:
- In theSystem Bannerat the top of the screen, tapAlarm Status Indicator
to open the Alarm Summary. - Atthe top of the Alarm Summary table, tapAlarm Manager
to open the Alarm Manager.
- From either theAlarm Summaryor theAlarm Manager, tapHelp
.
The
Help
popup shows all of the operations to perform on an alarm table. The buttons depicted in the popup include operations for the Alarm Summary
, Alarm Manager
, and Alarm History
. The Help
popup also displays a legend of icons for In Alarm/Unacknowledged, In Alarm/Acknowledged, Normal/Unacknowledged, and Faulted alarms.Available operations depend on the alarm screen:
Operation | Alarm Summary | Alarm Manager | Alarm History |
Acknowledge alarms | ![]() | ||
Disable alarms | ![]() | ![]() | |
Enable alarms | ![]() | ||
Filter alarms by Event Time | ![]() | ||
Pause the display of incoming alarms | ![]() | ||
Reset a digital alarm | ![]() | ||
Reset alarm counts | ![]() | ||
Select alarms | ![]() | ![]() | ![]() |
Shelve individual alarm conditions | ![]() | ![]() | |
Shelve entire alarm (all conditions) | ![]() | ||
Sort and filter alarms | ![]() | ![]() | ![]() |
View alarms | ![]() | ![]() | ![]() |
View alarm condition details | ![]() | ![]() | ![]() |
View alarm quality | ![]() | ![]() | |
Unshelve alarm conditions | ![]() | ||
Unshelve alarms | ![]() |
Provide Feedback