Help Popup Contents
The
on an HMI device. This popup shows a legend of icons that appear on the alarm screens and the task each button on an alarm table performs. The functions vary depending on the selected alarm table.
Help
popup opens when pressing Help
on an HMI device. This popup shows a legend of icons that appear on the alarm screens and the task each button on an alarm table performs. The functions vary depending on the selected alarm table.Help popup for Alarm Summary and Alarm Manager tables:

Help popup for Alarm History table:

Item | Description | |
![]() | A legend for icons in the alarm table. | |
![]() | A legend for alarm functions you can perform on the alarm table. The alarm functions represent buttons on the alarm table. The functions you can perform vary depending on the selected alarm table: | |
![]() | ![]() | Back opens the previously displayed screen. When opening the Alarm Manager screen from the Alarm Summary screen, this button reopens the Alarm Summary screen. |
![]() | Alarm Manager opens the Alarm Manager screen. The Alarm Manager lists all alarms configured in the system and their current states. Therefore, the Alarm Manager shows alarms not shown in the Alarm Summary , and provides additional tasks for alarms. | |
![]() | Details hides or shows the Details pane, which contains the details of the last selected alarm. The Details pane appears on the bottom half of large alarm tables and replaces the list of alarms in medium alarm tables. If no alarm is selected, the Details pane is empty. | |
![]() | Select All selects all of the alarms in the alarm table, including those not displayed on the current page of alarms. | |
![]() | Deselect All deselects all alarms in the alarm table, including those not displayed on the current page of alarms. | |
![]() | Select Page selects all of the alarms displayed on the current page of alarms. | |
![]() | Reset Latched Alarms sets the selected latched state of the alarm to Normal if the input of the alarm has returned to normal. Resetting a latched alarm acknowledges the alarm, if it is not acknowledged. | |
![]() | Reset Alarm Counts resets the alarm count in the controllers and the Alarm Count value in the Details pane of the Alarm Manager table to zero. The reset is performed for all conditions of the currently selected alarm. | |
![]() | Pause stops updates to the Alarm Summary table for 10 seconds or until performing another operation on the table. While updates to the Alarm Summary table are paused, alarms in the controllers are still evaluated. When the table is no longer paused, any changes to alarm states are reflected in the table and updates resume. | |
![]() | Disable stops the alarm condition from being evaluated. In effect, this turns off the selected alarm. This button disables the entire alarm. It is not possible to disable an individual alarm condition. | |
![]() | Enable enables the selected alarms in the Alarm Manager | |
![]() | Shelve prevents the notification of new state changes to the selected alarm if the alarm is acknowledged. Updates to the alarm do not appear. The alarm remains shelved until the shelve duration from the controller expires automatically or until manually unshelving the alarm. Updates to the alarm then resume. Shelving an alarm in the Alarm Summary table shelves only the selected alarm conditions. Shelving an alarm in the Alarm Manager table shelves all of the conditions of the alarm. From the condition list in the Details pane of the Alarm Manager table, shelve individual alarm conditions. Change the Shelve Duration and Max Shelve Duration using Logix Designer . Change the Shelve Duration and Max Shelve Duration values using Logix Designer in order to propagate updated values to the Alarm Summary and Alarm Manager clients. Use the previous Shelve Duration and Max Shelve Duration values when shelving alarms in Studio 5000 alarm tables. | |
![]() | Unshelve unshelves the selected alarm in the Alarm Manager table. Unshelving allows notification of new state changes to alarms. From the condition list in the Details pane of the Alarm Manager table, unshelve individual alarm conditions. | |
![]() | Acknowledge indicates that you are aware of the alarm. This button changes the state of the alarm from unacknowledged to acknowledged. | |
Date filter . Select the box and enter a date and time to list only the alarm state change records that occurred between the chosen date and time and the present. Select the checkbox on the right side to activate the filter. | ||
![]() | Refresh loads the latest alarm state changes from the alarm history. You can also exit and enter the screen with the Alarm History again to refresh with the latest changes. | |
![]() | Help opens this Help popup. | |
Provide Feedback