Alarm Summary table columns
Data fields in the
Alarm Summary
table appear in columns with descriptions of alarm information. The large Alarm Summary
table contains all columns by default. Medium Alarm Summary
tables contain a subset of the columns. The columns and their order depend on the configuration performed in
View Designer
. Data shown in the Details
pane may be added as a column in the Alarm Summary
table.Column | Description | Medium Alarm Summary | Large Alarm Summary |
! (Priority) | The urgency of the event:
| ![]() | ![]() |
Alarm State | The state of the alarm condition:
| ![]() | ![]() |
Inhibit State | The value applied to an alarm that inhibits the alarm at some level. These states include:
If no icon appears for Inhibit State, the alarm is of good quality and is not disabled, suppressed, or shelved. | ![]() | |
Event Time | The time the alarm condition or sub-condition changed to the currently displayed state. | ![]() | ![]() |
Condition Name | A name that describes the alarm condition. Condition names vary by event category. For example:
| ![]() | |
Alarm Name | The list of alarms, in all states, for the controllers referenced in the View Designer project. Each row contains an alarm and the conditions. Depending on configuration, the Alarm Name can appear as ::ControllerName.TagName or ::ControllerName\ProgramName.TagName. For tag-based alarms, the Alarm Name appears as ::ControllerName\ProgramName.TagName.@Alarms.AlarmName. If the tag is not located inside a program, this part is omitted and the Alarm Name appears as ::ControllerName.TagName.@Alarms.AlarmName. | ![]() | |
Message | The message assigned to the alarm in the alarm instruction. | ![]() | ![]() |
Provide Feedback