Alarm Manager screen
How do I open the Alarm Manager table?
In the
. The
. The
in the
System Banner
at the top of the screen, tap Alarm Status Indicator
. The Alarm Summary
screen opens. At the bottom of the Alarm Summary table, tap Alarm Manager
. The Alarm Manager
screen opens. You can open the Alarm Manager
screen from the Navigation menu
by tapping Navigation
in the System Banner
at the top of the screen and tapping the Alarm Manager
item in the Navigation menu
at the bottom of the screen.The
Alarm Manager
screen lists all alarms configured in the system and their current states. The Alarm Manager
subscribes to alarms in the controller and is used to monitor and interact with those alarms from the HMI device screen. Every alarm from every controller is listed unless an alarm is removed from the controller.Use the
Alarm Manager
to:- Enable or disable alarms to take them out of service
- Shelve and unshelve alarms
- Reset counts for alarms
- View details for a selected alarm or alarm condition
- Sort alarms
- Filter alarms
Provide Feedback