Alarm History for a medium HMI device screen
The
Alarm History Medium
alarm table is recommended for six-inch to nine-inch HMI device screens.
Item | Description | |
|---|---|---|
![]() | The list of alarm state changes records from the terminal. | |
![]() | Filter list. Select a filter in the HMI device to list only the alarm state change records containing the filter value for the indicated column. For example, if the filter exists, select the filter Priority:High to show only those alarm state changes with a high priority. Configure filters in View Designer . | |
![]() | Date filter. Select the box and enter a date and time to list only the alarm state change records that occurred between the chosen date and time and the present. Select the checkbox on the right side to activate the filter. | |
![]() | Number of filtered records and total number of records. | |
![]() | Buttons to perform actions available for the Alarm History Viewer: | |
![]() | Details hides or shows the Details pane, which contains the details of the last selected alarm state change record. The Details pane appears on the bottom half of large alarm tables and replaces the list of alarms in medium alarm tables. If no record is selected, the Details pane is empty. | |
![]() | Refresh loads the latest alarm state changes from the alarm history. The operator has to refresh the table to see the latest changes. The operator can also exit and enter the screen with the Alarm History again to refresh. | |
![]() | Help opens the Help popup. This popup displays a legend of icons and the task each button on an alarm table performs. | |
Provide Feedback